1109403_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1109403_en-US

1109403_en-US

HOWTO: Create APEX2 Project From Example in S32DS for Vision

S32DS for Vision contains many example projects from which you can learn how S32DS for Vision can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS for Vision. In this document, the procedure for creating a project from one of the provided APEX2 examples through to execution on the EVB is detailed.

1) Launch S32DS for Vision

2) Select 'New S32DS Project from example'

pastedImage_1.png

3) Select apex2_fast9 project

4) Click Finish

pastedImage_1.png

5) Change to C/C++ perspective, click on 'Switch to C/C++ Development'

pastedImage_6.png

6) Select apex2_fast9: A53 in the Project Explorer panel. Build the project using build config 'TEST_A53'.

pastedImage_1.png

7) Start a debug session using method as described in HOWTO: Create A53 Linux Project in S32DS for Vision, beginning at step 9.

Click Resume pastedImage_15.png

  • Should see something similar to what is pictured below
  • There are green diamonds at the corners in the image as identified by the fast9 corner detection algorithm

pastedImage_16.png

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-20-2025 07:20 AM
更新者: