1108991_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1108991_en-US

1108991_en-US

[Solution] IAR version 8.32 can not debug revision '1B' of LPC55S69 silicon

When you are the first time to debug LPC55S69, please read below document and double check your IDE, SDK and EVK version is correct.

Usually, we prefer use the latest IDE, SDK and EVK boards.

Important updates when using LPCXpresso55S69 Revision A2 boards and 1B silicon 

[Problem Description]

When you use IAR 8.32 to debug LPC55S69 '1B' silicon, the IDE will remind you "The debugging session could not be started", like below picture show:

debug_iar832.png

The reason of this failure is that IAR 8.32's LPC55S69 chip configuration files only support revision '0A' silicon, not '1B'.

We strongly recommend customer download and use IAR 8.40.2 or latest version. The IAR IDE start support LPC55S68 '1B' silicon from 8.40.2.

[Solution]

If you have some reasons that must use IAR 8.32, you can download attached zip file. This zip file like a patch, include the IAR LPC55S69 '1B' support files.

Un-zip this file and merge the same files under IAR installed path :IAR\arm\config\flashloader\NXP

Then the IAR can support '1B' silicons.

[How to identify LPC55(S)6x chip silicon versions]

On the top-side marking code, there is '1B'  charactors at the end of mark strings. See below two pictures, the left one is '1B' version chips.

                     LPC55(S)6x ver '1B'                                                               LPC55(S)6x ver '0A'

pastedImage_20.png                  pastedImage_21.png

LPC55xx
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-19-2025 02:48 PM
更新者: