s12zvml PMSM Sensorless Report Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s12zvml PMSM Sensorless Report Error

1,398件の閲覧回数
rzkity
Contributor II

Hello Everone!

   there is a problem relate to PMSM Sensorless ,when I use BDM DEBUG the motor program,The following error occurred, the error "xiaofan gu" Also mentioned,But I do according to file have no effect!

pastedImage_1.png

and the detail information is:

   pastedImage_2.png

I just add a LIN module into a project,and the LIN module is "FSL_LIN_2.x_STACK",but when i didnt do this,the project work well and can debug. but when i add the LIN module into the project, the problem occured.

I check it and find when i delete this "lin_isr.c" file,COMPLIE AND Debug OK,But LIN do not normal working!

So,what should i do?

Any help will be appreciated!

  thanks!

0 件の賞賛
返信
1 返信

1,323件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

Can you share with me the path of this file? There are 3 and you can choose the wrong one. Just to be sure.

Thank you.

Best Regards,

Diana

0 件の賞賛
返信