c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

c

1,335 Views
kendias
Contributor I

I am designing a control for a 4 phase motor with 4 coils fed @ 90 deg phase shift. All the NXP controls I see are 3 phase; however there are many motion control apps that use 4 phase i.e. turn tables, bikes etc. Mine is a PM motor. The chip I use is MC33033 which also actually does 4 phase control AND HAS 4 outputs for the 4 phases. Are there any NXP  devices that I can connect to the MC33033 to get 4 phase control? So all I do is connect my 4 motor coils to the NXP devices?

Tags (1)
0 Kudos
Reply
1 Reply

1,233 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, NXP doesn't provide 4 phase PMSM reference design.

Please check available PMSM reference design from NXP with below link:

Permanent Magnet Synchronous Motor (PMSM) Solutions|NXP 

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply