UDC-HI error while running a 24V PMSM with  DEVKIT-MOTORGD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UDC-HI error while running a 24V PMSM with  DEVKIT-MOTORGD

3,303 Views
steven_zhang
Contributor V

i cut the short-circuit line of J15 on DEVKIT-MOTORGD board so i can power the board and S32K144 board with an 24V adpter and driving a 24V PMSM. but i got UDC-HI error with below settings,how to set the voltage limitation for MCAD.

#define I_MAX (31.25F)
#define U_DCB_MAX (45.0F)
#define N_MAX (3500.0F)
#define WEL_MAX (1099.56F)
#define E_MAX (36.0F)

//Application Fault Triggers
//----------------------------------------------------------------------
#define U_DCB_TRIP (40.0F)
#define U_DCB_UNDER (16.0F)
#define U_DCB_OVER (30.0F)
#define I_PH_OVER (5.0F)
#define TEMP_OVER (110.0F)

 

 

 

UDC-HI.png

 

Tags (1)
0 Kudos
Reply
4 Replies

3,159 Views
Hartt4785
Contributor I

This community shares the information about motor control and smart energy in general. Control of all motor types: PMSM, BLDC, ACIM, SR and smart energy topics could be discussed.

0 Kudos
Reply

3,263 Views
marekmusak
NXP Employee
NXP Employee

I would recommend to download latest SW from product page:

https://www.nxp.com/mcspte1ak144

Nevertheless, could you make a snapshot of the FreeMASTER variable as below? 

marekmusak_0-1619534423851.png

Regards,

Marek

 

0 Kudos
Reply

3,287 Views
marekmusak
NXP Employee
NXP Employee

Hello Steven,

Thank you for contacting us. I would need more details to help you. 

Are those macros you printed here copied from MCAT tab - Output file or from PMSM_appconfig.h file?

Could you tell me version of the SW you are using? 

When does this fault occur? immediately or during motor operation?

Does it work at 12V?

Thanks!

Regards,

Marek

0 Kudos
Reply

3,277 Views
steven_zhang
Contributor V

thanks for your apllier

Are those macros you printed here copied from MCAT tab - Output file or from PMSM_appconfig.h file?-----from PMSM_appconfig.h ,but the macros are the same.

Could you tell me version of the SW you are using? ---------- S32DS for ARM 2018.R1 and MTRDEVKSPNK144_S32DS

When does this fault occur? immediately or during motor operation? -----immediately. 

Does it work at 12V?  ------it works at 12V for some low current motors such as a Linix.

0 Kudos
Reply