Metering

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Metering

1,839件の閲覧回数
RajPadmani
Contributor II

Hi community,

 

I'm working with the KM35 MCU and have implemented single-phase metering using the AN12837 application note. Calibration is complete, and I'm able to get accurate Vrms and Irms values.

 

I came across the following structure tMETERLIBLPRT1PH_DATA, which contains various metrology parameters such as ActPowers, AppPowers, PowerFactors, MetEnergyCounts, and MetEnergySecCounts.

 

I'm now looking to calculate the energy consumed (unit burned in kWh) based on these values.

 

My questions are:

 

Which parameters from this structure are directly relevant for calculating total energy consumption in kWh?

 

Is there a standard conversion or formula to go from MetEnergySecCounts[0] or ActPowers[0] to units consumed?

 

How frequently should I sample or accumulate values to get accurate energy readings over time?

 

Would really appreciate it if someone who's worked with KM35 or similar Freescale/NXP metering setups can guide me on how to make sense of this data for energy tracking.

 

Thanks in advance!

タグ(1)
0 件の賞賛
返信
1 返信

1,798件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @RajPadmani ,

Thanks for your post. Please refer to the AN13259.pdf. 

It contains detailed introductions to the APIs and parameters of the metering library, along with the corresponding calculation formulas.

Hope it can help you.

BRs,

Celeste

0 件の賞賛
返信