Evaluation board for BLDC control

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Evaluation board for BLDC control

4,986 次查看
cw26
Contributor I

Hey!

I need a development board that can run a 48V/1kW BLDC motor with sensored FOC implementation. Please suggest if you have any.

If you don't have any evaluation board for my specification, please suggest a suitable microcontroller and gate driver.

0 项奖励
回复
6 回复数

4,969 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

We have one development kit for 48V with options for S32K1 or S32K3 device.

But since the release will be next month I am not allowed to share details here on community.

If you could create ticket and state all the requirements I can share with your kit overview.

https://community.nxp.com/t5/HomeTest-Knowledge-Base/How-to-submit-a-new-question-for-NXP-Support/ta...

Best regards,

Peter

0 项奖励
回复

4,967 次查看
eCarMaker
Contributor III

Hi Peter, 

can the new development Kit be used with MPC5744P EVB Rev. E? I am also interested in.

Thanks in advance!

0 项奖励
回复

4,960 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

No, there are 2 options available:

S32K148 or S32K344

Best regards,

Peter

0 项奖励
回复

4,954 次查看
eCarMaker
Contributor III

Hi Peter,

I will reform my question. Right now I am using the power stage  Motor GD DevKit with MPC5744P EVB rev. E. Is there any other power stage, which is compatible with MPC5744P (just plugin) and has more power?

Thanks

 

 

0 项奖励
回复

4,926 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,
Yes, there is possibility but it will require some effort.
You can use MPC5744P EVB rev. E board, I expect you are referring to this one:

petervlna_0-1646743495155.png

You can connect this board to power stage via PCI:

https://www.nxp.com/design/designs/3-phase-reference-design-for-hybridpack-drive-igbt-sic-module-fea...

petervlna_1-1646743847399.png

you will need to cut the PCI cable and inset the wires into the devkit board connector. (the connector is standard)

Or to the :

https://www.nxp.com/design/designs/3-phase-reference-design-for-hp-drive-featuring-gd3160:RDGD3160I3...

Where you will need inverted from infineon: (for example)

https://www.digikey.at/de/products/detail/infineon-technologies/FS820R08A6P2BBPSA1/7324175?utm_adgro...

This one is compatible with our boards, so you will just push and connect it to it.

But all of this depends on the project budget and will require addition effort to get it running.

This is just a brief overview on possible solution.

Best regards,

Peter

 

 

0 项奖励
回复

4,908 次查看
eCarMaker
Contributor III

Hi Peter, 

Thanks for the detailed answer. Yes, you are right,  I am speaking about MPC5744P EVB rev. E .

  1. If I understand you correctly, the mentioned boards in the first and second links are just Gate Drivers for the IGBTs/MOSFETs e.g. FS820R08A6P2BBPSA1, which is mentioned in the third link. right?
  2. How about FRDM-MC-LVPMSM ? Is it compatible with MPC5744P EVB rev. E or we need to connect the signals individually?

Thanks in adavance!

 

 

0 项奖励
回复