Can I get the source code of an12200sw SpeedMeasure.h ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I get the source code of an12200sw SpeedMeasure.h ?

4,742 Views
clogordou
Contributor I

HI,all

   I used IMXT RT1052 development the dual servo , I have so problem  in speed measurement,and I get this AN12200SW demo help my works.  so i want get so detial in  SpeedMeasure.h of this function :

extern int32_tSpeedMeasure_F32_Calc(SPEED_MEASURE_F32_T *ptr);

Can you give me this function source code?

Thanks !

Labels (1)
Tags (2)
0 Kudos
Reply
7 Replies

4,576 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi clogord ou,

   Sorry for the later reply.

   I have got the information from our according department right now.

   The lib which you need is the critical functions and algorithm code, so we can't share with you directly.

    If you need it, you can contact with your local DFAE, and let the DFAE help you contact with the local NXP FAE, then you may get it.

   You can find your local distributor from this link:

Distributor Network | NXP 

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,576 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi clogord ou ,

   SpeedMeasure_F32_Calc function source code should in the speed_measure.a, and I also don't have it.

   If you want to get it, maybe you can provide your company and project information, then I can help you to check whether the source code can share with you or not from our internal side.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,576 Views
clogordou
Contributor I

Thanks for your help.

My company email : ouhuanchen@gzrobot.com

please send a email to me ,so i can reply for the project information.

thanks!

0 Kudos
Reply

4,576 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi clogord ou,

  I will help you to check it, any updated information will let you know.

 Please keep patient.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,576 Views
clogordou
Contributor I

Hi,Kerry Zhou

   Have U get this code? Can you give me some information ?

Thanks!

0 Kudos
Reply

4,576 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi clogord ou,

  I already help you to check it from our internal side, but still in the process, no feedback now, please keep patience.

  As you know, our related department also need time to check it.

  Any updated information, I will let you know.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

4,368 Views
dyereh
Contributor I

I also am looking for this source code as an example and to test out i.MX capability for real-time motor control. How can we acquire this?

0 Kudos
Reply