when open the file bldc_ref_sol.pmp in MCRSP_BLDC_V1.3.0/freemaster folder,pop up a error information:

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

when open the file bldc_ref_sol.pmp in MCRSP_BLDC_V1.3.0/freemaster folder,pop up a error information:

2,262件の閲覧回数
zhijunwu
Contributor I

Using FreeMaster 2.0, when open the file bldc_ref_sol.pmp in MCRSP_BLDC_V1.3.0/freemaster folder,pop up a error information:

   The associated file handle with C:\NXP\MCRSP_BLDC_V1.3.0\freemaster\bldc_ref_sol.pmp is incorrect.

and then close this information, FreeMaster also closed.

what's matter with it? open other .pmp file have not this problem.

the following picture is the real situation:

pastedImage_1.png

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,978件の閲覧回数
john_floros
NXP Employee
NXP Employee

What version of Freemaster are you using?  Try downloading the latest installation of Freemaster and install it.  It may fix you issue.  Once you have installed the latest version under help it should have the version 2.0.2.4  listed.

1,978件の閲覧回数
zhijunwu
Contributor I

Hi,John,

I update the FreeMaster version,and this problem have fixed,thank you for your adivce .

0 件の賞賛
返信