when I'm compiling an example of MBD, I got this error, Undefined function or variable 'lic_err'.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

when I'm compiling an example of MBD, I got this error, Undefined function or variable 'lic_err'.

ソリューションへジャンプ
1,754件の閲覧回数
jwsmarte
Contributor II
What should I do to get rid of it? Thanks! 
TIM图片20170916094650.png
ラベル(2)
0 件の賞賛
返信
1 解決策
1,430件の閲覧回数
jwsmarte
Contributor II

ok!Problem was solved with the following post.

HotFix_2: Fix license errors for DISK_SERIAL_NUM with less than 8 characters

NXP Tracking numberAST-619

 

Problem: If your HDD has a serial number with less than 8 characters, the license checking and validation will fail even if the license is correctly generated

 

Root Cause: Coding logic error

 

Workaround:  Update the file attached in the following folder 

{Toolbox install dir}\mbdtbx_pnt\mbdtbx_pnt\mscripts\matlab_ui\ folder mbd_pnt_hostid.p file

 

Customer Report: Undefined function or variable 'lic_err'.

元の投稿で解決策を見る

1 返信
1,431件の閲覧回数
jwsmarte
Contributor II

ok!Problem was solved with the following post.

HotFix_2: Fix license errors for DISK_SERIAL_NUM with less than 8 characters

NXP Tracking numberAST-619

 

Problem: If your HDD has a serial number with less than 8 characters, the license checking and validation will fail even if the license is correctly generated

 

Root Cause: Coding logic error

 

Workaround:  Update the file attached in the following folder 

{Toolbox install dir}\mbdtbx_pnt\mbdtbx_pnt\mscripts\matlab_ui\ folder mbd_pnt_hostid.p file

 

Customer Report: Undefined function or variable 'lic_err'.