when I'm compiling an example of MBD, I got this error, Undefined function or variable 'lic_err'.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

when I'm compiling an example of MBD, I got this error, Undefined function or variable 'lic_err'.

跳至解决方案
1,842 次查看
jwsmarte
Contributor II
What should I do to get rid of it? Thanks! 
TIM图片20170916094650.png
标签 (2)
0 项奖励
回复
1 解答
1,518 次查看
jwsmarte
Contributor II

ok!Problem was solved with the following post.

HotFix_2: Fix license errors for DISK_SERIAL_NUM with less than 8 characters

NXP Tracking numberAST-619

 

Problem: If your HDD has a serial number with less than 8 characters, the license checking and validation will fail even if the license is correctly generated

 

Root Cause: Coding logic error

 

Workaround:  Update the file attached in the following folder 

{Toolbox install dir}\mbdtbx_pnt\mbdtbx_pnt\mscripts\matlab_ui\ folder mbd_pnt_hostid.p file

 

Customer Report: Undefined function or variable 'lic_err'.

在原帖中查看解决方案

1 回复
1,519 次查看
jwsmarte
Contributor II

ok!Problem was solved with the following post.

HotFix_2: Fix license errors for DISK_SERIAL_NUM with less than 8 characters

NXP Tracking numberAST-619

 

Problem: If your HDD has a serial number with less than 8 characters, the license checking and validation will fail even if the license is correctly generated

 

Root Cause: Coding logic error

 

Workaround:  Update the file attached in the following folder 

{Toolbox install dir}\mbdtbx_pnt\mbdtbx_pnt\mscripts\matlab_ui\ folder mbd_pnt_hostid.p file

 

Customer Report: Undefined function or variable 'lic_err'.