the Parameter calculation does not match

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

the Parameter calculation does not match

4,038 次查看
董培董
Contributor II

hi ,

 When calculating the parameters of the observer, if the motor and electrical parameters are exactly the same, according to the method in the document(MC9S12ZVMMCLUG), the result calculated by MATLAB is different from the result calculated by MCAT. Is that accurate?The picture is as follows:

微信截图_20200921182715.png

微信截图_20200921183615.png

微信截图_20200921184242.png

微信截图_20200921184352.png

I want to get your help ,thank you very much!!!

 

0 项奖励
回复
5 回复数

3,945 次查看
Bark_8
Contributor I

thanks

0 项奖励
回复

3,949 次查看
Bark_8
Contributor I

Thanks for this info

0 项奖励
回复

4,001 次查看
nofake_drstrang
Contributor III

hi @董培董 ,

one question please:

 

do you use the example :

"\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop"

of the new toolbox version 1.4 

thanks in advance!

Best regards.

0 项奖励
回复

3,985 次查看
董培董
Contributor II

Hi, The soft version is as follows,and the FREEMASTER is 3.0,I hope I can get help,thank you very much

董培董_0-1601166193157.png

 

0 项奖励
回复

4,024 次查看
mariuslucianand
NXP Employee
NXP Employee

@marekmusak , can you please comment on this?

Thank you,

Marius

0 项奖励
回复