srec-MBD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

srec-MBD

1,635件の閲覧回数
abdelrhman
Contributor III

How to generate S record file of a simulink model instead of .elf file ??

0 件の賞賛
返信
2 返答(返信)

1,617件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @abdelrhman,

There is no need to do an extra conversion because the generated .mot file is in the .srec format.

Here is the line from our Makefile which generates the srec/mot file.

mariuslucianand_0-1658475503868.png

So, you can use directly the .mot file.

Hope this helps,

Marius

 

0 件の賞賛
返信

1,602件の閲覧回数
abdelrhman
Contributor III

where can I find the makefile location ?
some models does not generate the .mot files

0 件の賞賛
返信