s32k344 generate code error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32k344 generate code error

1,537 次查看
ca_liu
Contributor II

It's something wrong happened when I tried to generate code with s32ct for s32k344(footprint bga257),fault details are shown in the figure.And it seems to be related to the can module.When I delete the can module, the code can be generated normally, and the fault occurs again after adding it.

The version of s32ct is 1.4r,and it‘s installed automatically with mdbt (MBDToolbox_S32K3xx_1.1.0_20211220.mltbx)。

I hope I can get some help,thanks very much.

标记 (1)
0 项奖励
回复
0 回复数