s32k344 generate code error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k344 generate code error

1,567件の閲覧回数
ca_liu
Contributor II

It's something wrong happened when I tried to generate code with s32ct for s32k344(footprint bga257),fault details are shown in the figure.And it seems to be related to the can module.When I delete the can module, the code can be generated normally, and the fault occurs again after adding it.

The version of s32ct is 1.4r,and it‘s installed automatically with mdbt (MBDToolbox_S32K3xx_1.1.0_20211220.mltbx)。

I hope I can get some help,thanks very much.

タグ(1)
0 件の賞賛
返信
0 返答(返信)