s32k144 CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k144 CAN

Jump to solution
1,931 Views
Sriram
Contributor IV

Sriram_0-1656053736284.png

Hello , 

We are trying to run the CAN traffic example project from Nxp. But we are not getting any output while checking with the logic analyser. Do you have any feedback on how to get it running

 

 

0 Kudos
Reply
1 Solution
1,923 Views
SorinIBancila
NXP Employee
NXP Employee

Hello Sriram,

I have checked your model and I have a few questions about it:

  •  How did you download the code on the target? The checkbox 'Download Code after Build' seems to be disabled, so you must manually download the '.mot' file on the target. If you want to do this step automatically, you can simply enable the checkbox and then build again the model.

SorinIBancila_0-1656063399007.png

  • Did you power the board using a 12 V power supply (through J16) and set the jumper J107 to 1-2?

 

Best regards,

Bancila Sorin

View solution in original post

2 Replies
1,918 Views
Sriram
Contributor IV

Thanks for the reply , 

After selecting download code after build it worked.

We powered the board though j 16

0 Kudos
Reply
1,924 Views
SorinIBancila
NXP Employee
NXP Employee

Hello Sriram,

I have checked your model and I have a few questions about it:

  •  How did you download the code on the target? The checkbox 'Download Code after Build' seems to be disabled, so you must manually download the '.mot' file on the target. If you want to do this step automatically, you can simply enable the checkbox and then build again the model.

SorinIBancila_0-1656063399007.png

  • Did you power the board using a 12 V power supply (through J16) and set the jumper J107 to 1-2?

 

Best regards,

Bancila Sorin