s32k144 CAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,650件の閲覧回数
Sriram
Contributor IV

Sriram_0-1656053736284.png

Hello , 

We are trying to run the CAN traffic example project from Nxp. But we are not getting any output while checking with the logic analyser. Do you have any feedback on how to get it running

 

 

0 件の賞賛
返信
1 解決策
2,642件の閲覧回数
SorinIBancila
NXP Employee
NXP Employee

Hello Sriram,

I have checked your model and I have a few questions about it:

  •  How did you download the code on the target? The checkbox 'Download Code after Build' seems to be disabled, so you must manually download the '.mot' file on the target. If you want to do this step automatically, you can simply enable the checkbox and then build again the model.

SorinIBancila_0-1656063399007.png

  • Did you power the board using a 12 V power supply (through J16) and set the jumper J107 to 1-2?

 

Best regards,

Bancila Sorin

元の投稿で解決策を見る

2 返答(返信)
2,637件の閲覧回数
Sriram
Contributor IV

Thanks for the reply , 

After selecting download code after build it worked.

We powered the board though j 16

0 件の賞賛
返信
2,643件の閲覧回数
SorinIBancila
NXP Employee
NXP Employee

Hello Sriram,

I have checked your model and I have a few questions about it:

  •  How did you download the code on the target? The checkbox 'Download Code after Build' seems to be disabled, so you must manually download the '.mot' file on the target. If you want to do this step automatically, you can simply enable the checkbox and then build again the model.

SorinIBancila_0-1656063399007.png

  • Did you power the board using a 12 V power supply (through J16) and set the jumper J107 to 1-2?

 

Best regards,

Bancila Sorin