s32ct generate code error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32ct generate code error

1,798 次查看
ca_liu
Contributor II

It's something wrong happened when I tried to generate code with s32ct,fault details are shown in the figure.And it seems to be related to the can module.When I delete the can module, the code can be generated normally, and the fault occurs again after adding the module.

The version of s32ct is 1.4r,and it‘s installed automatically with mdbt (MBDToolbox_S32K3xx_1.1.0_20211220.mltbx)。And the chip is s32k344,footprint bga257.

I hope I can get some help,thanks very much.

标记 (1)
0 项奖励
回复
0 回复数