s32ct generate code error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32ct generate code error

1,792件の閲覧回数
ca_liu
Contributor II

It's something wrong happened when I tried to generate code with s32ct,fault details are shown in the figure.And it seems to be related to the can module.When I delete the can module, the code can be generated normally, and the fault occurs again after adding the module.

The version of s32ct is 1.4r,and it‘s installed automatically with mdbt (MBDToolbox_S32K3xx_1.1.0_20211220.mltbx)。And the chip is s32k344,footprint bga257.

I hope I can get some help,thanks very much.

タグ(1)
0 件の賞賛
返信
0 返答(返信)