problems with Gpt Notification 358 EBT example project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problems with Gpt Notification 358 EBT example project

1,826件の閲覧回数
XH
Contributor I

Hi there,

 

I encountered this problem with deploying the project " Gpt Notification 358 EBT example" to S32K358 processor, as shown in the attached image.

 

Could you please help?

 

Many thanks,

 

Xiaomei

0 件の賞賛
返信
1 返信

1,788件の閲覧回数
FlorinCiuca
NXP Employee
NXP Employee

Hello @XH !

 

From what I can see from the attached screenshot, it seems that the model you are trying to build is placed at a wrong path (C:\Users).

folder.pngfolder.png

It is very likely that you(or MATLAB) do(does) not have the correct privileges/write access in C:\Users. Please try to move the model at the path where your MATLAB projects are stored and re-build from there. Or if you did not make any changes to the model, you can try to build it directly from the Examples folder of the toolbox.

Best regards,

Florin.

0 件の賞賛
返信