.pmpx file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

.pmpx file

1,593 Views
paul_ephraim_13
Contributor III

Kindly elaborate on the genreration of the .pmpx file for a simulink model for real time data analysis.Screenshot 2024-09-06 134727.pngScreenshot 2024-09-06 132211.png

0 Kudos
Reply
2 Replies

1,521 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @paul_ephraim_13 

For creating a .pmpx file to watch the evolution of your variables inside FreeMASTER, please check Chapter 6 FreeMASTER PC application of the following article https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Sending-data-via-UART-and-monitoring-signa...

As I also see this article referenced in the image you have attached to the thread, could you please share with us if you encountered any issues in following the steps described in there?

Thank you,

Irina

0 Kudos
Reply

1,543 Views
agus_idiada
Contributor III

Hello Paul, may be I can help you, the file pmpx is the extension file of a freemaster project that has the information of the configuration you already did in freemaster. As far as I understand, you can not upload it into a simulink model. Freemaster is to watch variables of the DSP with a deployed code. Hope it helps.

0 Kudos
Reply