.pmpx file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

.pmpx file

803 次查看
paul_ephraim_13
Contributor III

Kindly elaborate on the genreration of the .pmpx file for a simulink model for real time data analysis.Screenshot 2024-09-06 134727.pngScreenshot 2024-09-06 132211.png

0 项奖励
回复
2 回复数

731 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hi @paul_ephraim_13 

For creating a .pmpx file to watch the evolution of your variables inside FreeMASTER, please check Chapter 6 FreeMASTER PC application of the following article https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Sending-data-via-UART-and-monitoring-signa...

As I also see this article referenced in the image you have attached to the thread, could you please share with us if you encountered any issues in following the steps described in there?

Thank you,

Irina

0 项奖励
回复

753 次查看
agus_idiada
Contributor III

Hello Paul, may be I can help you, the file pmpx is the extension file of a freemaster project that has the information of the configuration you already did in freemaster. As far as I understand, you can not upload it into a simulink model. Freemaster is to watch variables of the DSP with a deployed code. Hope it helps.

0 项奖励
回复