.pmpx file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

.pmpx file

1,592件の閲覧回数
paul_ephraim_13
Contributor III

Kindly elaborate on the genreration of the .pmpx file for a simulink model for real time data analysis.Screenshot 2024-09-06 134727.pngScreenshot 2024-09-06 132211.png

0 件の賞賛
返信
2 返答(返信)

1,520件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hi @paul_ephraim_13 

For creating a .pmpx file to watch the evolution of your variables inside FreeMASTER, please check Chapter 6 FreeMASTER PC application of the following article https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Sending-data-via-UART-and-monitoring-signa...

As I also see this article referenced in the image you have attached to the thread, could you please share with us if you encountered any issues in following the steps described in there?

Thank you,

Irina

0 件の賞賛
返信

1,542件の閲覧回数
agus_idiada
Contributor III

Hello Paul, may be I can help you, the file pmpx is the extension file of a freemaster project that has the information of the configuration you already did in freemaster. As far as I understand, you can not upload it into a simulink model. Freemaster is to watch variables of the DSP with a deployed code. Hope it helps.

0 件の賞賛
返信