nxp s32k358 MBDT how to custom Linker and startup code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nxp s32k358 MBDT how to custom Linker and startup code

Jump to solution
2,469 Views
jimmy623
Contributor I

Hi ,

    nxp s32k358 MBDT how to custom Linker and startup code?

I modify Pflash start address:

jimmy623_1-1719195786075.png

add customer linker file to setting path. 

jimmy623_0-1719195673983.png

run build, always failed.

jimmy623_2-1719195898479.png

how can i fix this issue?

Thanks!

 

 

0 Kudos
Reply
1 Solution
2,367 Views
dragostoma
NXP Employee
NXP Employee

Hi, @jimmy623,

Recently, the last version of S32K3 Toolbox was released, namely version 1.5.0. Try an installation of this version and check if you still have problems using the custom linker.
It is worth mentioning instead that if the intention is to use the S32K3 toolbox together with the BMS toolbox, which work together, they are functional for the moment only in version 1.4.0 of the S32K3 toolbox.

Let us know if your problem persists.

 

Regards,

Dragos

View solution in original post

0 Kudos
Reply
4 Replies
2,395 Views
dragostoma
NXP Employee
NXP Employee

Hi, @jimmy623,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

What version of K3 toolbox are you currently using? Do you intend to use the K3 toolbox together with the BMS toolbox on your S32K358 board or just the general standalone K3 toolbox?

I ask because I have not yet succeeded in reproducing your problem and it would be helpful to know what environment it was tested on.

 

Best regards,

Dragos

 

0 Kudos
Reply
2,381 Views
jimmy623
Contributor I

Hi ,

Thank you for your attention,

toolbox version:

 Model-Based Design Toolbox for S32K3xx Series version 1.4.0 (RFP)

0 Kudos
Reply
2,368 Views
dragostoma
NXP Employee
NXP Employee

Hi, @jimmy623,

Recently, the last version of S32K3 Toolbox was released, namely version 1.5.0. Try an installation of this version and check if you still have problems using the custom linker.
It is worth mentioning instead that if the intention is to use the S32K3 toolbox together with the BMS toolbox, which work together, they are functional for the moment only in version 1.4.0 of the S32K3 toolbox.

Let us know if your problem persists.

 

Regards,

Dragos

0 Kudos
Reply
2,247 Views
jimmy623
Contributor I
update SW32_MBDT_S32K3xx 1.4.0 to 1.5.0. it works!
Thanks!
0 Kudos
Reply