bsc9132 network card drive In the Linux kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bsc9132 network card drive In the Linux kernel

2,278件の閲覧回数
zhengguangzhe
Contributor I

There are bsc9132 network card drivers related to TX, RX four-way matching on the Linux kernel how corresponding, how is the corresponding interface configured?

address:psc9132 

タグ(1)
0 件の賞賛
返信
1 返信

2,195件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello zhengguangzhe‌,

Here on the Model-Based Design community we handle questions regarding our toolbox or other MATLAB/Simulink related questions. I think your question is best suited for the Qonverge community, so my advice is to ask it there (as I can not move it myself).

Hope this helps,

Razvan.

0 件の賞賛
返信