XTAL frequency selection in S32K model based design toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

XTAL frequency selection in S32K model based design toolbox

1,592件の閲覧回数
hemantsindkar
Contributor III

Hi,

How to select XTAL frequency in S32K model based design toolbox other than 8MHz or 40MHz? There are only two selections 8MHz and 40MHz.

pastedImage_1.png

pastedImage_2.png

Thanks

Hemant S.

0 件の賞賛
返信
1 返信

1,469件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi hemantsindkar‌,

In model based design - we have the selection only for the option that exist on NXP development boards. Right now you can't select other frequencies since there is no way for us to tested. We will have a new release in October 2017 and we are considering your input in this matter.

I've logged this as: AST-708

Thank you!

Daniel

0 件の賞賛
返信