XTAL frequency selection in S32K model based design toolbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XTAL frequency selection in S32K model based design toolbox

1,602 Views
hemantsindkar
Contributor III

Hi,

How to select XTAL frequency in S32K model based design toolbox other than 8MHz or 40MHz? There are only two selections 8MHz and 40MHz.

pastedImage_1.png

pastedImage_2.png

Thanks

Hemant S.

0 Kudos
Reply
1 Reply

1,479 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi hemantsindkar‌,

In model based design - we have the selection only for the option that exist on NXP development boards. Right now you can't select other frequencies since there is no way for us to tested. We will have a new release in October 2017 and we are considering your input in this matter.

I've logged this as: AST-708

Thank you!

Daniel

0 Kudos
Reply