XCP support for S32K144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

XCP support for S32K144

2,339 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi all,

are there plans to support XCP functionality in the model-based design toolbox for S32K144?.

Thanks,

Lukas

0 项奖励
回复
4 回复数

805 次查看
ltt-be
Contributor I

Hello, where can I find an XCP calibration sample project for the S32K144 ?

0 项奖励
回复

1,992 次查看
KalaimaniArumugamdev
Contributor III

Hi,

   First of all s32k support XCP functionality.(THIS IS MENTIONED IN "MBD Approach with MATLAB & SIMULINK
in Powertrain Application Development
Using NXP Microprocessor S32Kxx" slide number 9.

Also refer https://community.nxp.com/t5/S32K/S32K144-XCP-on-CAN/m-p/1225059/highlight/true#M9802

 

 

1,996 次查看
bolei
Contributor II

hello Lukas, have you figured it out, is there any documentations/meterials about that you can share?

thanks, 

bo

0 项奖励
回复

2,248 次查看
constantinrazva
NXP Employee
NXP Employee

Hello lukaszadrapa,

For now there are no plans to support XCP.

Kind regards,

Razvan.

0 项奖励
回复