Why MBD ToolBox just only one "Timer block"?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why MBD ToolBox just only one "Timer block"?

2,019 次查看
niequanwei
Contributor III

When I used the MBD ToolBox ,I just find that there was only one "Timer Block" 

1.jpg

However, the reference manual sheet has two timers.

2.jpg

Meanwhile, there are many registers, and I just don't know how to configure it from the that block,such as"How to select one of the timers" and so on.

标记 (4)
2 回复数

1,897 次查看
constantinrazva
NXP Employee
NXP Employee

Hello niequanwei@aochutec.com‌,

This is an older toolbox and it only supports one timer block. Unfortunately we do not have a newer version for the MCU you are using. Our newer releases (like S32K14x) support many more peripherals, so if that's of interest to you, please take a look.

Kind regards,

Razvan.

1,897 次查看
niequanwei
Contributor III

Got it ! Thank you!

0 项奖励
回复