What do the words 8D and 94 on the variable capacitance diode model BBY40 mean.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What do the words 8D and 94 on the variable capacitance diode model BBY40 mean.

2,633件の閲覧回数
zgy
Contributor I

What do the words 8D and 94 on the variable capacitance diode model BBY40 mean.

We have a unit that has an index of scanning fast lock code. According to the production feedback, some boards can't be scanned. There are differences in the positioning of this device. There are several batches of devices on the line. The printing is somewhat different. We use a capacitance meter to measure the results. The results are different. I want to know the reasons for the differences.

20200226133411.jpg20200226133356.jpg20200226133428.jpgThis is the difference between the test results with a capacitance meter. The voltage given by the capacitance meter is about 1.3V,94, give the same voltage, 94 has a larger capacitance. In some cases, a small amount of capacitance is needed. At this time, the voltage applied at 94 is larger than other ones20200226133439.jpg

ラベル(4)
0 件の賞賛
返信
1 返信

2,574件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

This community space do not cover the topic you need assistance on.

Please create new thread on the https://community.nxp.com/community/other  community space or new NXP support case according to following procedure:https://community.nxp.com/docs/DOC-329745

 

Hope this helps,

Marius

0 件の賞賛
返信