Using MBDT in Simulink Projects with "Refresh Simulink customizations" option enabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using MBDT in Simulink Projects with "Refresh Simulink customizations" option enabled

跳至解决方案
3,302 次查看
mks004
Contributor II

I am running into an issue when I try to access the MBDT library from the Simulink Library Browser. Everything works as expected when I open a Simulink model and access the Library Browser, i.e. I can see the MBDT blocks in the Library Browser. However when I add the same Simulink model to a Simulink Project with "Refresh Simulink customizations" configuration option enabled, open the model from the project view, and then access the Library Browser, the MBDT blocks are no longer there. All other library blocks still show up as expected.

I use these versions of software:
MATLAB R2020a Update 7
NXP_MBDToolbox_S32K1xx 4.2.0

This issue manifests itself with any model I open. Any help is appreciated.

0 项奖励
回复
1 解答
3,275 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @mks004 ,

Can you please press the F5 button when you open the Simulink library?

If a window appears, select the second option, smth with Generate ... in memory. I am sorry, I cannot reproduce that window now.

Hope this helps,

Marius

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,262 次查看
mks004
Contributor II

Hello @mariuslucianand ,

This works, thank you.

0 项奖励
回复
3,276 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @mks004 ,

Can you please press the F5 button when you open the Simulink library?

If a window appears, select the second option, smth with Generate ... in memory. I am sorry, I cannot reproduce that window now.

Hope this helps,

Marius

0 项奖励
回复