Use segger J-link instead of openSDA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use segger J-link instead of openSDA

1,523件の閲覧回数
theopubben
Contributor I

Within simulink i can select a com port or openSDA to download code to the target. Is it possible to use a J-link from Segger for this purpose?

Thank you.

0 件の賞賛
返信
1 返信

1,262件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Theo, 

The Simulink can only download (for the moment) via UART type protocols. Hence you cannot use JTAG based protocols directly from Simulink - BUT - you may generate and built the application from Simulink and get the elf/mot/srec file associated with the application and downloaded via the J-link using an external debugger such as S32 Design Studio that support the JTAG based protocols.

Hope this helps!

Daniel

0 件の賞賛
返信