Use MBDT to Configurate MPC5775B and MC33771C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use MBDT to Configurate MPC5775B and MC33771C

1,228 Views
Albert228
Contributor II

Hello everyone,

I found that MC33771 MBD toolbox is given under S32K1 tool .And I found the advice about the configuration of MPC5744 and MC33772B (MPC5744P &MC33771B Configuration)

Now I want to use MBDT to establish model to configurate MPC577B and MC33771C. I want to know if there is a corresponding tool chain now.

If there is not tool , could someone provide a demo or description file to help me build model to connect MPC577B and MC33771C?

Look forward to your reply.

2.png

Thank you!

0 Kudos
Reply
3 Replies

1,163 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @Albert228,

Unfortunately, for the MPC we do not provide any ready to be added blocks to control the BCCs and also we do not have any ready to run examples using custom code.

However, the article you have mentioned MPC5744P-and-MC33771-Configuration  alongside the article mentioned on How-to-use-your-own-C-code-in-our-Toolbox-Battery-Management are the proper materials to guide you on how to use custom code to communicate between MPC33775B and MC33771 B/C. You could start from the MPC5744 example, change the hardware part, and then identify the SPI interfaces alongisde their pins. 

Hope this helps,

Marius

 

 

0 Kudos
Reply

962 Views
Albert228
Contributor II

Hello @mariuslucianand

I followed the way  MPC5744P-and-MC33771-Configuration and download the archive, and open the model in R2022b.The model could be built when the MCU is set to MPC5744p.However,when the MCU is set to MPC577B,an error is displayed in the next picture.

4.png2.png

I found that 'SIUL0_CLK'used in 'mbdt_utils.c' declared in the file of 'MPC5744P_features.h'.I think I should use 'MPC5775B_features.h' in my project.But  'SIUL0_CLK'  undeclared in the file of 'MPC5775B_features.h'. So should I modify the file of  'mbdt_utils.c'?What should I do to modify the file?

5.png

Thank you.

0 Kudos
Reply

991 Views
Albert228
Contributor II

Hello Marius,

I followed the way  MPC5744P-and-MC33771-Configuration and download the archive, and open the model in R2022b.The model could be built when the MCU is set to MPC5744p.However,when the MCU is set to MPC577B,an error is displayed in the next picture.4.png2.png

 

What should I do to finish the build when the MCU is set to MPC5775b?

Thank you.

0 Kudos
Reply