Unable to install the Model based design toolbox.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to install the Model based design toolbox.

ソリューションへジャンプ
11,307件の閲覧回数
1312765191
Contributor I

Dear engineer,

 I encountered the same problem as Cannot install Model based design toolbox because *.mltbx file missing 。I want to know if you have solved this problem now,If yes, please give me some help。

best fishes

1 解決策
11,086件の閲覧回数
1312765191
Contributor I

Thanks a lot, i get it!Just modify the downloaded file ".zip" to ".mltbx" and drag it to the matlab command line.

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
11,087件の閲覧回数
1312765191
Contributor I

Thanks a lot, i get it!Just modify the downloaded file ".zip" to ".mltbx" and drag it to the matlab command line.

0 件の賞賛
返信
11,086件の閲覧回数
sandeepsandeepk
Contributor II

how to convert .zip to .mltbx. i am having issue in this step.

0 件の賞賛
返信
11,086件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected],

You can just rename the file from <toolbox>.zip to <toolbox>.mltbx 

You can right click the file -> properties and in the general tab you find the name (in the example below the name is lpuart_s32k_transmit and the extension is .tlc; just rename the extension).

pastedImage_2.png

Hope this clears things up a bit.

Kind regards,

Razvan.

0 件の賞賛
返信
11,086件の閲覧回数
sandeepsandeepk
Contributor II

Actually the .zip extenction in that is not there. and even in that if I made in change it will be like .zip.mktbx extenction

Screenshot (71).png

0 件の賞賛
返信
11,086件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

On Windows, in File Explorer, go to View and check the File name extensions. Now it will display the file name and its extension.

pastedImage_1.png

Now you can change the .zip extension file to mltbx.

Hope this helps,

Marius

0 件の賞賛
返信
10,190件の閲覧回数
mv3234
Contributor II

thanks sir ,it works ,

0 件の賞賛
返信
11,085件の閲覧回数
sandeepsandeepk
Contributor II

Thanks it worked.

11,085件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Basically there are two ways of installing the toolbox.

1. The approach that you are trying and the one mentioned in the thread that you sent us is to manually download the product from here https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=11703517. As my colleague, constantinrazvan.chivu mentioned in that thread, if it is downloaded as .zip archive you simply have to change the extension from the .zip to .mltbxpastedImage_1.png

2. The second approach is to go to Matlab AddOns, search "NXP" and follow the steps for the tool that you are interested in.

pastedImage_2.png

Hope this helps,

Marius