Unable to active MBD Toolbox

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to active MBD Toolbox

跳至解决方案
702 次查看
Vast-Horizon
Contributor II

Hello,

I'm trying to go through the installation process of MBD Toolbox 1.1.0, but it fail to verify the license.

VastHorizon_0-1726266220775.png

I do have a license on the nxp website and I can download thelicense.dat file but that doesn't work.

The thing is, It worked before on my old laptop, but I got a new laptop recently and I wanted to install these packages back. Maybe that's the reason? 

VastHorizon_1-1726266622086.png

VastHorizon_2-1726266668662.png

 

 

 

 

 

 

0 项奖励
回复
1 解答
665 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @Vast-Horizon,

Usually, Error Code -9 means that the license file is correctly attached to the toolbox, but something is wrong with it.

Most likely, if you say that it worked on an older computer and now it doesn't work on the new computer, it may be because you are trying to use the same generated license file, because I see that the license you want to use is generated in the month of May.

The license is generated based on the HostID - your machine's volume partition's serial number. Use the vol command on the Command Prompt to find this serial number.

A single MBDT license associated with a single machine can be generated for each NXP account. You will need to return the license and create a new one linked to the new computer if you choose to switch the machine on which you want to use it.

I hope this solves your license activation problem.

 

Best regards,

Dragos

在原帖中查看解决方案

0 项奖励
回复
1 回复
666 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @Vast-Horizon,

Usually, Error Code -9 means that the license file is correctly attached to the toolbox, but something is wrong with it.

Most likely, if you say that it worked on an older computer and now it doesn't work on the new computer, it may be because you are trying to use the same generated license file, because I see that the license you want to use is generated in the month of May.

The license is generated based on the HostID - your machine's volume partition's serial number. Use the vol command on the Command Prompt to find this serial number.

A single MBDT license associated with a single machine can be generated for each NXP account. You will need to return the license and create a new one linked to the new computer if you choose to switch the machine on which you want to use it.

I hope this solves your license activation problem.

 

Best regards,

Dragos

0 项奖励
回复