Torque control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Torque control

2,147件の閲覧回数
bhanu_kassel
Contributor II

Hi dumitru-daniel.popa ,

I am using two user buttons as torque commands. For example , when I am running the motor at zero speed or any speed and apply some torque command, if we try to rotate the wheel and we can feel the applied torque. For every half revoultion of the rotor , torque is going to zero and again gaining his torque. Torque is not present at 0 and 180 degrees position. I need to get applied torque at zero and 180 degrees position also.  How can i resolve this issue? What are the other soultions for this problem?

Best Regards,

Bhanu 

0 件の賞賛
返信
1 返信

1,992件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Are you saying the motor has no torque for half of the electrical period ? Then how it could turn ?

0 件の賞賛
返信