Torque control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Torque control

2,044 Views
bhanu_kassel
Contributor II

Hi dumitru-daniel.popa ,

I am using two user buttons as torque commands. For example , when I am running the motor at zero speed or any speed and apply some torque command, if we try to rotate the wheel and we can feel the applied torque. For every half revoultion of the rotor , torque is going to zero and again gaining his torque. Torque is not present at 0 and 180 degrees position. I need to get applied torque at zero and 180 degrees position also.  How can i resolve this issue? What are the other soultions for this problem?

Best Regards,

Bhanu 

0 Kudos
Reply
1 Reply

1,889 Views
Daniel_Popa
NXP Employee
NXP Employee

Are you saying the motor has no torque for half of the electrical period ? Then how it could turn ?

0 Kudos
Reply