Switching between Run mode and High Speed Run mode - using model based design

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Switching between Run mode and High Speed Run mode - using model based design

1,214 次查看
Sriram
Contributor IV

Hello,

 I m using s32k146 mcu and using matlab model based design. I need some help with EEE write. Currently the program is running is HSRUN mode (112Mhz clk) but i want use EEE write which i think is only possible in RUN mode (80MHz) . Can you pls specify the steps to change the mode from HSRUN to RUN in matlab model based design.

 

Thanks

MBDT #s32k146

标记 (2)
0 项奖励
回复
0 回复数