Switching between Run mode and High Speed Run mode - using model based design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Switching between Run mode and High Speed Run mode - using model based design

1,213件の閲覧回数
Sriram
Contributor IV

Hello,

 I m using s32k146 mcu and using matlab model based design. I need some help with EEE write. Currently the program is running is HSRUN mode (112Mhz clk) but i want use EEE write which i think is only possible in RUN mode (80MHz) . Can you pls specify the steps to change the mode from HSRUN to RUN in matlab model based design.

 

Thanks

MBDT #s32k146

タグ(2)
0 件の賞賛
返信
0 返答(返信)