Suspected FlexCAN library error on MPC5744, when transferring with extension ID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Suspected FlexCAN library error on MPC5744, when transferring with extension ID

1,518件の閲覧回数
youngkugpark
Contributor III

Dear All

As shown in the title, there is no problem when receiving a message with an extended ID using MPC 5744p EVB, but when transmitting using the CAN Transmitter provided by MBDT, it is confirmed in the CAN Monitoring Tool that the extended ID is recognized as a standard ID even though it is checked as shown in the attached picture.
Is there an error in the CAN transmitter block like I think?
Or what am I missing?
For your information, ID 351 and 352 are sending using the extended ID

0 件の賞賛
返信
0 返答(返信)