Simulink no configuration block for MPC57xx!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simulink no configuration block for MPC57xx!

Jump to solution
2,851 Views
60010001
Contributor II

Screenshot (274).png

it occurs when i drag block model to workspace ,How to fix it?

I follow Quick Start Guide but didn't do 1.2.3 Setting up the Target Compiler because i don't know where it is.

1 Solution
2,732 Views
constantinrazva
NXP Employee
NXP Employee

Hello 60010001@kmitl.ac.th,

You have to first put a Main configuration block inside your model - this is the block where you set up what MCU you are using from the MPC57xx family, compiler options, download options, etc. This block is used by most of the other blocks, as they need to know what options are available for the MCU you've selected (e.g.: what pins are available for the certain peripheral on that MCU).

Kind regards,

Razvan.

View solution in original post

3 Replies
2,733 Views
constantinrazva
NXP Employee
NXP Employee

Hello 60010001@kmitl.ac.th,

You have to first put a Main configuration block inside your model - this is the block where you set up what MCU you are using from the MPC57xx family, compiler options, download options, etc. This block is used by most of the other blocks, as they need to know what options are available for the MCU you've selected (e.g.: what pins are available for the certain peripheral on that MCU).

Kind regards,

Razvan.

2,732 Views
60010001
Contributor II

Thank you 

0 Kudos
Reply
2,732 Views
constantinrazva
NXP Employee
NXP Employee

Glad I could help you!

KR,

Razvan.