Simulink no configuration block for MPC57xx!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simulink no configuration block for MPC57xx!

ソリューションへジャンプ
3,677件の閲覧回数
60010001
Contributor II

Screenshot (274).png

it occurs when i drag block model to workspace ,How to fix it?

I follow Quick Start Guide but didn't do 1.2.3 Setting up the Target Compiler because i don't know where it is.

1 解決策
3,558件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected],

You have to first put a Main configuration block inside your model - this is the block where you set up what MCU you are using from the MPC57xx family, compiler options, download options, etc. This block is used by most of the other blocks, as they need to know what options are available for the MCU you've selected (e.g.: what pins are available for the certain peripheral on that MCU).

Kind regards,

Razvan.

元の投稿で解決策を見る

3 返答(返信)
3,559件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected],

You have to first put a Main configuration block inside your model - this is the block where you set up what MCU you are using from the MPC57xx family, compiler options, download options, etc. This block is used by most of the other blocks, as they need to know what options are available for the MCU you've selected (e.g.: what pins are available for the certain peripheral on that MCU).

Kind regards,

Razvan.

3,558件の閲覧回数
60010001
Contributor II

Thank you 

0 件の賞賛
返信
3,558件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Glad I could help you!

KR,

Razvan.