Similink Network Vehicle Tools box integrated with NXP CAN Unpack/Pack Blocks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Similink Network Vehicle Tools box integrated with NXP CAN Unpack/Pack Blocks

2,954件の閲覧回数
PaulSMagna
Contributor II

The NXP S32K1 Similink Tool box has an ISR that provides the CAN interface to the CAN Message buffers. The output of the block does not have the complete message available. 

The Similink Tool box, Network Vehicle has an interface to unpack a Complete Msg frame and there seems now to be needed a block between them that re-assembles the CAN message so this tool box can be effectively used. This is the same issue for the Pack block and the NXP Send Block, there is not proper interface for them to plug and play together

image.png

 

image.png

 

0 件の賞賛
返信
3 返答(返信)

2,909件の閲覧回数
PaulSMagna
Contributor II
We found a solution by using the Pack to get the CAN msg structure for the Unpack . and Unpack to get the data for the Pack

2,910件の閲覧回数
PaulSMagna
Contributor II

So have found a solution to the issue by using the 

using the Pack to get the CAN Msg Structure for the Unpack . and Unpack to get the data for the Pack

0 件の賞賛
返信

2,926件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

@paulvlase , could you please have a look on @PaulSMagna 's question?

Regards,

Marius

0 件の賞賛
返信