S32ZE MBDT mTopR52_SPF_multiCPU example issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32ZE MBDT mTopR52_SPF_multiCPU example issue

1,926 Views
Wei_H
Contributor III

Hi,

I've encountered issue with trying to compile and generate code for example project, "mTopR52_SPF_multiCPU".

This the error I'm getting:

Wei_H_0-1760571920372.png

So I tried running the script:

mbd_s32ze_build_multicore('mTopR52_SPF2_MultiCPU')

but I got the following error:

Unrecognized field name "Core_type".

Error in mbd_s32ze_build_multicore>@(x)mbd_s32ze.nxp.target.get_target_core(x.Core_type)

Error in mbd_s32ze_build_multicore

0 Kudos
Reply
1 Reply

1,823 Views
vladmitroi
NXP Employee
NXP Employee

Hello,

What MATLAB version are you using ? You might try to run the mbd_s32ze_path script in command line, followed by a sl_refresh_customization and restart MATLAB. 
Also, verify that multicore is enabled from Hw Settings->Hardware Implementation->Multicore and try building with Build Selected Nodes button.

As a notice, for using the SPF2 core, a premium license is needed and a processor with DSP/ML option enabled. Please contact NXP sales team if you do not have such a license.

vladmitroi_0-1761222446769.png

 

0 Kudos
Reply