S32K344 - What does the Adc_Calibrate function in the ADC block do?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 - What does the Adc_Calibrate function in the ADC block do?

1,466 Views
rishikesh_c
Contributor III

I am developing a model on Simulink with MBDT 1.3. In the ADC block, there is one function called Adc_Calibrate. What does this function do?

I put it in an enabled subsystem and this is the output - raw data from one of the ADC blocks on the same AdcHwUnit as the one selected with Adc_Calibrate:

1 - When the subsystem is enabled, the raw values look like this on FreeMASTER:

rishikesh_c_0-1711960537857.png


And when it is not enabled, it looks like this:

rishikesh_c_1-1711963406181.png


It is a similar graph but the difference is in the maximum values it reaches. When the subsystem is not enabled, the maximum value it reaches is about 150 and when it is enabled it reaches around 1400. 

What is the reason for this and what exactly is the purpose of the Adc_Calibrate function?

Thanks

 

Tags (4)
0 Kudos
Reply
2 Replies

1,289 Views
stefanvlad
NXP Employee
NXP Employee

Hello Rishi Chapekar and Amol Parikh,

 

The Adc_Calibrate function inside the ADC blocks implements the ADC Calibration activity, that can be added in the Initialize Subsystem:

stefanvlad_0-1714052953497.png

The Adc_Calibrate function will help the ADC peripheral to minimize the reading errors and get closer to the Ideal response:

stefanvlad_0-1714062940864.png

Figure 3. Effect of calibration error on ADC response 

 

An in-depth analysis of the recommended ADC calibration can be found here: 16-bit SAR ADC calibration - NXP Community

 

It is recommended to use the ADC Calibration block only in the Initialization part of the model, otherwise running it in a repeated triggered subsystem will result in the values getting filtered as your results.

 

Best practices to increase the ADC accuracy can be found also in AN12217: S32K1xx ADC guidelines, specs, and configuration – Application Note (nxp.com).

 

Best regards,

Stefan V.

0 Kudos
Reply

1,404 Views
AmolParikh
Contributor I

I am also facing the same problem, does anyone have any solution for it?

 

0 Kudos
Reply