S32K344 PIL timeout error while receiving data from the rtiostream interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 PIL timeout error while receiving data from the rtiostream interface

1,171件の閲覧回数
sh_dhanasekaran
Contributor II

Hi, 

I work with MATLAB 2022b and on target board S32K344-Q257. I have been trying to run the Simple PiL s32ct. 

Even though I get a message that 'the executable file has been downloaded to S32K344'

I end up with the following error!

The timeout of 10 seconds for receiving data from the rtiostream interface has been exceeded. There might be multiple reasons for this failure.
You should:

a) Check that the target hardware configuration is correct

b) Confirm that the target is running

c) Consider the possibility of application run-time failure, consider using SiL, which supports signal handlers and debugging

If you cannot find a solution, consider using the method setTimeoutRecvSecs of rtw.connectivity.RtIOStreamHostCommunicator to increase the timeout value.

0 件の賞賛
返信
0 返答(返信)