S32K312 CAN configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 CAN configuration

Jump to solution
4,453 Views
paul_14
Contributor I

Hello, I have developed a code using Matlab/Simulink MBDT to echo CAN messages (the echoed message has a CAN ID equal to the received message CAN ID + 1).

I use PCAN-View to send to and receive from the board. This is S32K312-Q172.

This works OK for messages with extended CAN IDs, but not for standard IDs.

To receive CAN messages on the board, I use CanIf_RxIndication.

To send CAN messages from the board, I use CanHardwareObject_Can0_Tx_Interrupt with the following configuration:

  • Can Implementation Type: FULL
  • Can ID Message Type: MIXED
  • In the simulink mask of the Can_Write block, the "Extended ID CAN Message" option is unchecked

I also use a CanIf_TxConfirmation block.

 

Could you please provide some guidance to make my code work for both types of CAN Messages IDs?

0 Kudos
Reply
1 Solution
4,229 Views
robertv
NXP Employee
NXP Employee

Hello Pablo,

I looked at your model and I think I found a solution for your issue.

What I ultimately had to do was to set Can ID Message Type either to STANDARD or EXTENDED, for the RECEIVE objects. By keeping one of them as a polling hardware object, the MainFunction_Read is still necessary. 

I chose STANDARD for CanHardwareObject_Can0_Rx_Std_Polling (id=1) and EXTENDED CanHardwareObject_Can0_Rx_Ext_Interrupt (id=2) (instead of MIXED). 

 Screenshot 2025-03-03 185902.png

With these changes alone I got the model to work in the following way:
- Sent EXTENDED frame from Can Analyzer - > started receiving EXTENDED frame messages with the ID incremented by 1 from the board
- Sent STANDARD frame from Can Analyzer - > started receiving EXTENDED frame messages with the ID incremented by 1 from the board

In case you are looking to also reply with the same message type, then you would need to implement a workflow that includes 2 Can_Write blocks (one with the checkbox for Extended enabled and one without), and based on the received frame, you redirect to the content to the appropriate Can_Write.

A few ideas on how you could differentiate between the frames:
- By received ID length, but this might be tricky depending on how this is stored
- By Hardware Object ID: going back to the configuration referenced above, CanHardwareObject with the ID 1 was set to receive STANDARD messages, so if your received CAN message comes from the object with the ID 1, you know it's a STANDARD message; otherwise if it's ID 2, then you know it was captured by the can hardware object with ID 2, configured to receive EXTENDED frames.

Please let me know if this fixes the issue you were encountering. 

Regards,
Robert V

View solution in original post

0 Kudos
Reply
7 Replies
4,412 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @paul_14 

As a first step, could you please try and set the CAN ID Message Type for the Receive Hardware Object on MIXED?

mixed rx.png

After this setting is performed, as illustrated above, could you please try and rebuild the model and check if you are able to receive messages with both EXTENDED and STANDARD IDs?

Thank you,

Irina

0 Kudos
Reply
4,400 Views
paul_14
Contributor I

Hi @Irina_Costachescu 

Yes, I already had this CAN Hw Object with message type as MIXED.

I have all these CAN Objects:

0. CanHardwareObject_Can0_Rx_FIFO: FULL/MIXED/RECEIVE

1. CanHardwareObject_Can0_Rx_Std_Polling: BASIC/MIXED/RECEIVE

2. CanHardwareObject_Can0_Rx_Ext_Interrupt: BASIC/MIXED/RECEIVE

3. CanHardwareObject_Can0_Tx_Polling: BASIC/MIXED/TRANSMIT

4. CanHardwareObject_Can0_Tx_Interrupt: BASIC/MIXED/TRANSMIT

 

And this is how my model looks like:

paul_14_0-1739802761637.png

 

Thanks,

Pablo

0 Kudos
Reply
4,281 Views
robertv
NXP Employee
NXP Employee

Hello @paul_14 , 

I tried to replicate a scenario similar to what you have here.

First of all, using the default configuration (no changes) that comes with the Toolbox for the S32K312-Q172, i managed to send both EXTENDED and STANDARD frames simply by checking and unchecking the "Extended ID Can Message" property inside the CAN_Write block. Additionally, I tried using the same Can Hardware Object (CanHardwareObject_Can0_Tx_Interrupt) to send EXTENDED and STANDARD frames on alternate execution steps.

Where I think I noticed a possible inconvenient was when trying to receive both STANDARD and EXTENDED frames, where it seemed like only the EXTENDED frames were being received. That happens because of the way the hardware objects are configured:
- CanHardwareObject_Can0_Rx_Ext_Interrupt is able to receive EXTENDED frames, and it's configured to work based on interrupts, meaning  there is nothing else you have to do in order for the message to be captured by the Hardware Interrupt Callback set to CanIf_RxIndication. 
- CanHardwareObject_Can0_Rx_Std_Polling is able to receive STANDARD frames, and it's configured to work based on the polling mechanism, meaning that in order for this to trigger the Hardware Interrupt Callback, an additional block is needed, that being the Can Block set to Can_MainFunction_Read. This triggers the aforementioned Hardware Interrupt Callback when the hardware object set to polling is receiving messages.
Screenshot 2025-02-27 122258.png

Setting the Can ID Message Type to MIXED might not lead to the desired results when using the RECEIVE objects because MIXED is treated as EXTENDED for this case. 

I see the following options, to be able to RECEIVE both EXTENDED and STANDARD frames:
- use the configuration provided by default and also add a Can_MainFunction_Read block into your model, triggering the interrupt for the polling can hardware object
- modify the polling hardware object to work on interrupts instead:
Screenshot 2025-02-27 121925.png

Let me know if these explanations help you and if you manage to get the model to work as expected. 

Regards,
Robert V

0 Kudos
Reply
4,241 Views
paul_14
Contributor I

Hi @robertv ,

I'm afraid I've tried both options and none of the get my code to work with standard IDs.

I'm attaching my model so hopefully you can have a look at it.

Many thanks,

Pablo

0 Kudos
Reply
4,230 Views
robertv
NXP Employee
NXP Employee

Hello Pablo,

I looked at your model and I think I found a solution for your issue.

What I ultimately had to do was to set Can ID Message Type either to STANDARD or EXTENDED, for the RECEIVE objects. By keeping one of them as a polling hardware object, the MainFunction_Read is still necessary. 

I chose STANDARD for CanHardwareObject_Can0_Rx_Std_Polling (id=1) and EXTENDED CanHardwareObject_Can0_Rx_Ext_Interrupt (id=2) (instead of MIXED). 

 Screenshot 2025-03-03 185902.png

With these changes alone I got the model to work in the following way:
- Sent EXTENDED frame from Can Analyzer - > started receiving EXTENDED frame messages with the ID incremented by 1 from the board
- Sent STANDARD frame from Can Analyzer - > started receiving EXTENDED frame messages with the ID incremented by 1 from the board

In case you are looking to also reply with the same message type, then you would need to implement a workflow that includes 2 Can_Write blocks (one with the checkbox for Extended enabled and one without), and based on the received frame, you redirect to the content to the appropriate Can_Write.

A few ideas on how you could differentiate between the frames:
- By received ID length, but this might be tricky depending on how this is stored
- By Hardware Object ID: going back to the configuration referenced above, CanHardwareObject with the ID 1 was set to receive STANDARD messages, so if your received CAN message comes from the object with the ID 1, you know it's a STANDARD message; otherwise if it's ID 2, then you know it was captured by the can hardware object with ID 2, configured to receive EXTENDED frames.

Please let me know if this fixes the issue you were encountering. 

Regards,
Robert V

0 Kudos
Reply
4,209 Views
paul_14
Contributor I

Hi Robert,

I managed to get my model working with your suggestions, receiving and echoing both standard and extended ID CAN messages.

Thank you!!

Pablo

0 Kudos
Reply
4,196 Views
robertv
NXP Employee
NXP Employee

Hello Pablo,

I'm glad to hear it worked.
And thank you for confirming the solution was successful!

Regards,
Robert V

0 Kudos
Reply
%3CLINGO-SUB%20id%3D%22lingo-sub-2044459%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ES32K312%20CAN%20configuration%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2044459%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHello%2C%20I%20have%20developed%20a%20code%20using%20Matlab%2FSimulink%20MBDT%20to%20echo%20CAN%20messages%20(the%20echoed%20message%20has%20a%20CAN%20ID%20equal%20to%20the%20received%20message%20CAN%20ID%20%2B%201).%3C%2FP%3E%3CP%3EI%20use%20PCAN-View%20to%20send%20to%20and%20receive%20from%20the%20board.%20This%20is%20%3CSTRONG%3ES32K312-Q172%3C%2FSTRONG%3E.%3C%2FP%3E%3CP%3EThis%20works%20OK%20for%20messages%20with%20extended%20CAN%20IDs%2C%20but%20not%20for%20standard%20IDs.%3C%2FP%3E%3CP%3ETo%20receive%20CAN%20messages%20on%20the%20board%2C%20I%20use%20%3CSTRONG%3ECanIf_RxIndication%3C%2FSTRONG%3E.%3C%2FP%3E%3CP%3ETo%20send%20CAN%20messages%20from%20the%20board%2C%20I%20use%26nbsp%3B%3CSTRONG%3ECanHardwareObject_Can0_Tx_Interrupt%3C%2FSTRONG%3E%20with%20the%20following%20configuration%3A%3C%2FP%3E%3CUL%3E%3CLI%3ECan%20Implementation%20Type%3A%20FULL%3C%2FLI%3E%3CLI%3ECan%20ID%20Message%20Type%3A%20MIXED%3C%2FLI%3E%3CLI%3EIn%20the%20simulink%20mask%20of%20the%20Can_Write%20block%2C%20the%20%22Extended%20ID%20CAN%20Message%22%20option%20is%20unchecked%3C%2FLI%3E%3C%2FUL%3E%3CP%3EI%20also%20use%20a%26nbsp%3B%3CSTRONG%3ECanIf_TxConfirmation%3C%2FSTRONG%3E%26nbsp%3Bblock.%3C%2FP%3E%3CBR%20%2F%3E%3CP%3ECould%20you%20please%20provide%20some%20guidance%20to%20make%20my%20code%20work%20for%20both%20types%20of%20CAN%20Messages%20IDs%3F%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2055617%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20S32K312%20CAN%20configuration%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2055617%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHello%20Pablo%2C%3C%2FP%3E%0A%3CP%3EI'm%20glad%20to%20hear%20it%20worked.%3CBR%20%2F%3EAnd%20thank%20you%20for%20confirming%20the%20solution%20was%20successful!%3CBR%20%2F%3E%3CBR%20%2F%3ERegards%2C%3CBR%20%2F%3ERobert%20V%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2055392%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20S32K312%20CAN%20configuration%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2055392%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%20Robert%2C%3C%2FP%3E%3CP%3EI%20managed%20to%20get%20my%20model%20working%20with%20your%20suggestions%2C%20receiving%20and%20echoing%20both%20standard%20and%20extended%20ID%20CAN%20messages.%3C%2FP%3E%3CP%3EThank%20you!!%3C%2FP%3E%3CP%3EPablo%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2054866%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20S32K312%20CAN%20configuration%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2054866%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHello%20Pablo%2C%3C%2FP%3E%0A%3CP%3EI%20looked%20at%20your%20model%20and%20I%20think%20I%20found%20a%20solution%20for%20your%20issue.%3C%2FP%3E%0A%3CP%3EWhat%20I%20ultimately%20had%20to%20do%20was%20to%20set%20Can%20ID%20Message%20Type%20either%20to%20STANDARD%20or%20EXTENDED%2C%20for%20the%20RECEIVE%20objects.%20By%20keeping%20one%20of%20them%20as%20a%20polling%20hardware%20object%2C%20the%20MainFunction_Read%20is%20still%20necessary.%26nbsp%3B%3C%2FP%3E%0A%3CP%3EI%20chose%20%3CSTRONG%3ESTANDARD%3C%2FSTRONG%3E%20for%20CanHardwareObject_Can0_Rx_Std_Polling%20(id%3D1)%20and%20%3CSTRONG%3EEXTENDED%3C%2FSTRONG%3E%20CanHardwareObject_Can0_Rx_Ext_Interrupt%20(id%3D2)%20(%3CSTRONG%3Einstead%20of%20MIXED%3C%2FSTRONG%3E).%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%26nbsp%3B%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22Screenshot%202025-03-03%20185902.png%22%20style%3D%22width%3A%20441px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22Screenshot%202025-03-03%20185902.png%22%20style%3D%22width%3A%20441px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F326509iCF40FF719F7FE394%2Fimage-dimensions%2F441x271%3Fv%3Dv2%22%20width%3D%22441%22%20height%3D%22271%22%20role%3D%22button%22%20title%3D%22Screenshot%202025-03-03%20185902.png%22%20alt%3D%22Screenshot%202025-03-03%20185902.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3EWith%20these%20changes%20alone%20I%20got%20the%20model%20to%20work%20in%20the%20following%20way%3A%3CBR%20%2F%3E-%20Sent%20EXTENDED%20frame%20from%20Can%20Analyzer%20-%20%26gt%3B%20started%20receiving%20EXTENDED%20frame%20messages%20with%20the%20ID%20incremented%20by%201%20from%20the%20board%3CBR%20%2F%3E-%20Sent%20STANDARD%20frame%20from%20Can%20Analyzer%20-%20%26gt%3B%20started%20receiving%20EXTENDED%20frame%20messages%20with%20the%20ID%20incremented%20by%201%20from%20the%20board%3CBR%20%2F%3E%3CBR%20%2F%3EIn%20case%20you%20are%20looking%20to%20also%20reply%20with%20the%20same%20message%20type%2C%20then%20you%20would%20need%20to%20implement%20a%20workflow%20that%20includes%202%20Can_Write%20blocks%20(one%20with%20the%20checkbox%20for%20Extended%20enabled%20and%20one%20without)%2C%20and%20based%20on%20the%20received%20frame%2C%20you%20redirect%20to%20the%20content%20to%20the%20appropriate%20Can_Write.%3C%2FP%3E%0A%3CP%3EA%20few%20ideas%20on%20how%20you%20could%20differentiate%20between%20the%20frames%3A%3CBR%20%2F%3E-%20%3CSTRONG%3EBy%20received%20ID%20length%3C%2FSTRONG%3E%2C%20but%20this%20might%20be%20tricky%20depending%20on%20how%20this%20is%20stored%3CBR%20%2F%3E-%20%3CSTRONG%3EBy%20Hardware%20Object%20ID%3C%2FSTRONG%3E%3A%20going%20back%20to%20the%20configuration%20referenced%20above%2C%20CanHardwareObject%20with%20the%20ID%201%20was%20set%20to%20receive%20STANDARD%20messages%2C%20so%20if%20your%20received%20CAN%20message%20comes%20from%20the%20object%20with%20the%20ID%201%2C%20you%20know%20it's%20a%20STANDARD%20message%3B%20otherwise%20if%20it's%20ID%202%2C%20then%20you%20know%20it%20was%20captured%20by%20the%20can%20hardware%20object%20with%20ID%202%2C%20configured%20to%20receive%20EXTENDED%20frames.%3C%2FP%3E%0A%3CP%3EPlease%20let%20me%20know%20if%20this%20fixes%20the%20issue%20you%20were%20encountering.%26nbsp%3B%3CBR%20%2F%3E%3CBR%20%2F%3ERegards%2C%3CBR%20%2F%3ERobert%20V%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2054604%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20S32K312%20CAN%20configuration%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2054604%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F219933%22%20target%3D%22_blank%22%3E%40robertv%3C%2FA%3E%26nbsp%3B%2C%3C%2FP%3E%3CP%3EI'm%20afraid%20I've%20tried%20both%20options%20and%20none%20of%20the%20get%20my%20code%20to%20work%20with%20standard%20IDs.%3C%2FP%3E%3CP%3EI'm%20attaching%20my%20model%20so%20hopefully%20you%20can%20have%20a%20look%20at%20it.%3C%2FP%3E%3CP%3EMany%20thanks%2C%3C%2FP%3E%3CP%3EPablo%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2052913%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20S32K312%20CAN%20configuration%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2052913%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHello%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F227365%22%20target%3D%22_blank%22%3E%40paul_14%3C%2FA%3E%26nbsp%3B%2C%26nbsp%3B%3C%2FP%3E%0A%3CP%3EI%20tried%20to%20replicate%20a%20scenario%20similar%20to%20what%20you%20have%20here.%3C%2FP%3E%0A%3CP%3EFirst%20of%20all%2C%20using%20the%20default%20configuration%20(no%20changes)%20that%20comes%20with%20the%20Toolbox%20for%20the%20S32K312-Q172%2C%20i%20managed%20to%20send%20both%20EXTENDED%20and%20STANDARD%20frames%20simply%20by%20checking%20and%20unchecking%20the%20%22Extended%20ID%20Can%20Message%22%20property%20inside%20the%20CAN_Write%20block.%20Additionally%2C%20I%20tried%20using%20the%20same%20Can%20Hardware%20Object%20(CanHardwareObject_Can0_Tx_Interrupt)%20to%20send%20EXTENDED%20and%20STANDARD%20frames%20on%20alternate%20execution%20steps.%3C%2FP%3E%0A%3CP%3EWhere%20I%20think%20I%20noticed%20a%20possible%20inconvenient%20was%20when%20trying%20to%20receive%20both%20STANDARD%20and%20EXTENDED%20frames%2C%20where%20it%20seemed%20like%20only%20the%20EXTENDED%20frames%20were%20being%20received.%20That%20happens%20because%20of%20the%20way%20the%20hardware%20objects%20are%20configured%3A%3CBR%20%2F%3E-%20%3CSTRONG%3ECanHardwareObject_Can0_Rx_Ext_Interrupt%3C%2FSTRONG%3E%20is%20able%20to%20receive%20EXTENDED%20frames%2C%20and%20it's%20configured%20to%20work%20based%20on%20interrupts%2C%20meaning%26nbsp%3B%20there%20is%20nothing%20else%20you%20have%20to%20do%20in%20order%20for%20the%20message%20to%20be%20captured%20by%20the%20Hardware%20Interrupt%20Callback%20set%20to%20CanIf_RxIndication.%26nbsp%3B%3CBR%20%2F%3E-%20%3CSTRONG%3ECanHardwareObject_Can0_Rx_Std_Polling%3C%2FSTRONG%3E%20is%20able%20to%20receive%20STANDARD%20frames%2C%20and%20it's%20configured%20to%20work%20based%20on%20the%20polling%20mechanism%2C%20meaning%20that%20in%20order%20for%20this%20to%20trigger%20the%20Hardware%20Interrupt%20Callback%2C%20an%20additional%20block%20is%20needed%2C%20that%20being%20the%20Can%20Block%20set%20to%20%3CSTRONG%3ECan_MainFunction_Read%3C%2FSTRONG%3E.%20This%20triggers%20the%20aforementioned%20Hardware%20Interrupt%20Callback%20when%20the%20hardware%20object%20set%20to%20polling%20is%20receiving%20messages.%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22Screenshot%202025-02-27%20122258.png%22%20style%3D%22width%3A%20393px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22Screenshot%202025-02-27%20122258.png%22%20style%3D%22width%3A%20393px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F326052iDBB8626159847F18%2Fimage-dimensions%2F393x260%3Fv%3Dv2%22%20width%3D%22393%22%20height%3D%22260%22%20role%3D%22button%22%20title%3D%22Screenshot%202025-02-27%20122258.png%22%20alt%3D%22Screenshot%202025-02-27%20122258.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3ESetting%20the%20Can%20ID%20Message%20Type%20to%20MIXED%20might%20not%20lead%20to%20the%20desired%20results%20when%20using%20the%20RECEIVE%20objects%20because%20%3CSTRONG%3EMIXED%20is%20treated%20as%20EXTENDED%20for%20this%20case%3C%2FSTRONG%3E.%26nbsp%3B%3C%2FP%3E%0A%3CP%3EI%20see%20the%20following%20options%2C%20to%20be%20able%20to%20RECEIVE%20both%20EXTENDED%20and%20STANDARD%20frames%3A%3CBR%20%2F%3E-%20use%20the%20configuration%20provided%20by%20default%20and%20also%20add%20a%20Can_MainFunction_Read%20block%20into%20your%20model%2C%20triggering%20the%20interrupt%20for%20the%20polling%20can%20hardware%20object%3CBR%20%2F%3E-%20modify%20the%20polling%20hardware%20object%20to%20work%20on%20interrupts%20instead%3A%3CBR%20%2F%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22Screenshot%202025-02-27%20121925.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22Screenshot%202025-02-27%20121925.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F326051i68E6F1E229900DCC%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22Screenshot%202025-02-27%20121925.png%22%20alt%3D%22Screenshot%202025-02-27%20121925.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3ELet%20me%20know%20if%20these%20explanations%20help%20you%20and%20if%20you%20manage%20to%20get%20the%20model%20to%20work%20as%20expected.%26nbsp%3B%3CBR%20%2F%3E%3CBR%20%2F%3ERegards%2C%3CBR%20%2F%3ERobert%20V%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2045566%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20S32K312%20CAN%20configuration%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2045566%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F100054%22%20target%3D%22_blank%22%3E%40Irina_Costachescu%3C%2FA%3E%26nbsp%3B%3C%2FP%3E%3CP%3EYes%2C%20I%20already%20had%20this%20CAN%20Hw%20Object%20with%20message%20type%20as%20MIXED.%3C%2FP%3E%3CP%3EI%20have%20all%20these%20CAN%20Objects%3A%3C%2FP%3E%3CP%3E0.%26nbsp%3BCanHardwareObject_Can0_Rx_FIFO%3A%20FULL%2FMIXED%2FRECEIVE%3C%2FP%3E%3CP%3E1.%26nbsp%3BCanHardwareObject_Can0_Rx_Std_Polling%3A%20BASIC%2FMIXED%2FRECEIVE%3C%2FP%3E%3CP%3E2.%20CanHardwareObject_Can0_Rx_Ext_Interrupt%3A%20BASIC%2FMIXED%2FRECEIVE%3C%2FP%3E%3CP%3E3.%20CanHardwareObject_Can0_Tx_Polling%3A%20BASIC%2FMIXED%2FTRANSMIT%3C%2FP%3E%3CP%3E4.%20CanHardwareObject_Can0_Tx_Interrupt%3A%20BASIC%2FMIXED%2FTRANSMIT%3C%2FP%3E%3CBR%20%2F%3E%3CP%3EAnd%20this%20is%20how%20my%20model%20looks%20like%3A%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22paul_14_0-1739802761637.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22paul_14_0-1739802761637.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F324323iA105F63D6695C09B%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22paul_14_0-1739802761637.png%22%20alt%3D%22paul_14_0-1739802761637.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3CP%3EThanks%2C%3C%2FP%3E%3CP%3EPablo%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2045396%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20S32K312%20CAN%20configuration%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2045396%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F227365%22%20target%3D%22_blank%22%3E%40paul_14%3C%2FA%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3EAs%20a%20first%20step%2C%20could%20you%20please%20try%20and%20set%20the%20CAN%20ID%20Message%20Type%20for%20the%20Receive%20Hardware%20Object%20on%20%3CSTRONG%3EMIXED%3C%2FSTRONG%3E%3F%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22mixed%20rx.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22mixed%20rx.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F324267i989D78A65E44EF97%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22mixed%20rx.png%22%20alt%3D%22mixed%20rx.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3EAfter%20this%20setting%20is%20performed%2C%20as%20illustrated%20above%2C%20could%20you%20please%20try%20and%20rebuild%20the%20model%20and%20check%20if%20you%20are%20able%20to%20receive%20messages%20with%20both%20EXTENDED%20and%20STANDARD%20IDs%3F%3C%2FP%3E%0A%3CP%3EThank%20you%2C%3C%2FP%3E%0A%3CP%3EIrina%3C%2FP%3E%3C%2FLINGO-BODY%3E