S32K148EVB - Simulink - External Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148EVB - Simulink - External Mode

ソリューションへジャンプ
4,829件の閲覧回数
mfarag
Contributor II

Dear Sir/Madam,

I am trying the run the Simulink example of External Model (see photo below) on the S32K148EVB.

pastedImage_1.png

I am able to build the model (see image below):

pastedImage_2.png

When I click "connect to the target" button, I usually receive that error (see image below):

pastedImage_3.png

pastedImage_4.png

Kindly find below image of the model configurations:

pastedImage_1.png

Can someone help?

Thanks,

Mohammed Farag

ラベル(2)
1 解決策
4,376件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi mfarag‌,

Someone in our team will look over this and reply you later on. A quick tip: can you try with a lower UART baud rate?

Also, are you absolutely sure the board is connected via COM Port 13 ? Just check in your Windows OS Device Manager on which COM Port the board is communicating with.

Thank you!

Daniel

元の投稿で解決策を見る

2 返答(返信)
4,377件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi mfarag‌,

Someone in our team will look over this and reply you later on. A quick tip: can you try with a lower UART baud rate?

Also, are you absolutely sure the board is connected via COM Port 13 ? Just check in your Windows OS Device Manager on which COM Port the board is communicating with.

Thank you!

Daniel

4,376件の閲覧回数
mfarag
Contributor II

Thanks dumitru-daniel.popa‌

Changed the COM port to the one specified by the Windows OS Device Manager and lowered the UART baud rate. It's working now