S32K1 MBD CAN Message Lost after Disconnection from BusMaster

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K1 MBD CAN Message Lost after Disconnection from BusMaster

660 次查看
ykarata1
Contributor IV

Dear All,

I am using Model Based Design with S32K144 DEVKIT. I have implemented CAN communication. My communication block are typically categorized under two title.

1. 28 piece TX message

2. 1 piece RX message

 

When I build the model, code is embedded to the DEVKIT and I can see the all TX messages on my CAN line from BUSMASTER. 

The problems that I have are:

When I disconnect via BUSMASTER and if that time is bigger than 1 sec as far as I measure, It never sends any of the TX messages. I need to reset again to see any CAN Signal. 

 

My questions:

 

1. What may be the reason of this failure?

2. How can I solve that?

Any help will be appreciated.

Thanks.

 

NOTE: I could not share my model. If needed please let me know on e-mail.

ykarata1_0-1603705791384.png

 

 

 

 

0 项奖励
回复
0 回复数