MBDT for Simulink - Generate Licenses - What to Put in Name Field?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT for Simulink - Generate Licenses - What to Put in Name Field?

Jump to solution
1,554 Views
rsating
Contributor III

When creating a license for the NXP Model Based Design Toolbox for Simulink, we have to create a license on the NXP website as shown below in the attached screenshot.  What is the purpose of the "Name" field?  Name of the machine?  Or something else?  Is entry in the field optional? Or required for activation to succeed?

Following the link "Instructions for finding your host ID details are available here." did not help answer the question.

Thanks

NXP_MBDT_Generate-Licenses_fields.png

0 Kudos
Reply
1 Solution
1,542 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @rsating ,

You can type any name there. I think the purpose of that field is to add a brief text note to your license. Just the Disk Serial number has to be the correct one.

Hope this helps,

Marius

View solution in original post

0 Kudos
Reply
1 Reply
1,543 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @rsating ,

You can type any name there. I think the purpose of that field is to add a brief text note to your license. Just the Disk Serial number has to be the correct one.

Hope this helps,

Marius

0 Kudos
Reply